Blog - JLC3DP
3D Printing Design3D Printing KnowledgeCNC Machining KnowledgeCNC Machining Design
How to Add Colors to STL Files
STL files typically contain only geometric information (vertices and triangles) and don't inherently store color data. So when you only have STL files, but want to produce color 3D printed parts, you need to colorize your stl files first and export color print files that can be put into production directly . To colorize an STL file, you'll need to associate color information with the vertices or faces of the model. (About How to generate STL file, please check it here:STL file) General guide on how yo......
Mar 20,2024
Is There Any Recommended 3D Design Software?
Autodesk AutoCAD Autodesk AutoCAD is a versatile and widely-used software for 2D and 3D computer-aided design (CAD) and drafting. Known for its precision and comprehensive toolset, AutoCAD is essential for architects, engineers, and construction professionals. It supports parametric design, allowing users to create and modify objects based on a set of rules, enhancing accuracy and efficiency. AutoCAD also integrates well with other Autodesk products and offers features like DWG file compatibility, ext......
May 18,2024
Unlocking 10 Secrets for Mastery in 3D Print Modeling
Fellow 3D printing enthusiasts, do you often find 3D modeling to be a headache? Today, I will reveal the secrets that make modeling masters thrive! By mastering these ten techniques, you will easily grasp the essence of modeling, transforming every idea into a vivid 3D masterpiece! Technique 1: Simplify Model Structure Remove Redundant Details: At the beginning of the modeling process, avoid adding too many unnecessary details. Focus on capturing the main features and shapes of the object. Use Low-Pol......
May 17,2024
How To Create And Construct Your Own 3D Printer
The world of 3D printing is a captivating realm where imagination becomes reality. While there are numerous commercially available 3D printers, why not embark on a thrilling journey and create your own? Building a 3D printer from scratch not only offers a unique sense of accomplishment but also provides an opportunity to unleash your creativity and delve into the intricacies of this transformative technology. So, if you're ready to embark on an exciting journey of creating your own 3D printer, let's d......
Apr 29,2024
Choosing the Right 3D Printing Material: A Guide to Making the Best Material Selection
To get the intended outcomes from your 3D printing projects, selecting a suitable material is fundamental. Given the variety of materials that are accessible, it's critical to take into account attributes like strength, flexibility, durability, heat resistance, and aesthetics etc. Which kind of material works best for your project? Although it's difficult to tell for sure, your parts will turn out better the more you understand the available possibilities and the characteristics of different materials......
Apr 28,2024
How to Generate STL File for PCB Enclosures at EasyEDA
EasyEDA Pro, the upgraded version of EasyEDA, introduced several enhanced features, and one noteworthy improvement is the advanced 3D CAD function. In this article, we'll delve into utilizing this feature effectively. (Video tutorial) Simplifying 3D Housing Design &Export Flexibility EasyEDA Pro facilitates the creation of simple 3D housings, empowering users to swiftly sketch and construct uncomplicated enclosures for their projects,and also EasyEDA Pro allows you to export the design in STEP or OBJ ......
Mar 20,2024
How to Add Colors to STL Files
STL files typically contain only geometric information (vertices and triangles) and don't inherently store color data. So when you only have STL files, but want to produce color 3D printed parts, you need to colorize your stl files first and export color print files that can be put into production directly . To colorize an STL file, you'll need to associate color information with the vertices or faces of the model. (About How to generate STL file, please check it here:STL file) General guide on how yo......
Mar 20,2024
Taking Your Nylon 3D Prints to the Next Level: Exploring Post-Processing Methods
Importance of Nylon 3d printing Post-processing Post-processing plays a crucial role in nylon 3D printing by offering several important benefits. Firstly, it enhances the strength and durability of nylon parts. Nylon 3D-printed items frequently need to be post-processed to increase their strength and longevity. Heat treatment, for instance, can make nylon parts more crystalline, which improves their stiffness and strength. By eliminating internal tensions, post-processing can further increase the dura......
Feb 28,2024
Seamless Perfection: The Ultimate Guide to Vapor Smoothing in 3D Printing
What Is Vapor Smoothing and How it Works? In 3D printing, vapor smoothing is a post-processing method used to enhance manufactured objects' surface smoothness. The printed object is exposed to vaporized solvent during the process, which reacts with the plastic to make it dissolve and re-flow somewhat and produce a smoother surface. To smooth the vapor, the printed object is placed within a sealed container or chamber. A solvent is injected into the chamber and allowed to vaporize and fill the space, s......
Feb 27,2024
Exploring the World of 3D Wax Printing: Applications, Pros, and Cons
Understanding 3D Wax Printing 3D wax printing is an additive manufacturing process using wax-based materials to create three-dimensional stuff. Making a computerized, three-dimensional model of the intended product and cutting it into thin layers are the steps in the procedure. The sliced model is then sent to a 3D printer that can work with wax materials. The printer deposits or melts the wax layer by layer, following the instructions from the sliced model. Support structures may be used if needed. P......
Jan 27,2024
Exploring the Potential of FDM for Flexible 3D Printing
What is flexible 3D printing? The term "flexible 3D printing" describes the technique of producing three-dimensional goods with materials that have elasticity and may compress, bend, or stretch. FDM 3D Printing Flexible FDM 3D printing makes use of Fused Deposition Modelling (FDM) to create three-dimensional things out of flexible and elastic materials. varying degrees of flexibility and durability can be produced by adapting FDM printers to accept flexible filaments such as thermoplastic elastomers (......
Jan 27,2024
Wood Filament for 3D Printing: Composition, Print Settings, Applications, Pros, and Cons
3D printing with wood filament is a fascinating application of additive manufacturing technology that allows you to create objects with the appearance and properties of wood. Wood filament is a composite material made by combining a base polymer, such as PLA (polylactic acid), with finely ground wood fibers or particles. Filament composition and Print settings The composition of wood filament typically involves a combination of wood particles or fibers and a biodegradable polymer, such as PLA (polylac......
Jan 26,2024
Injection Molding vs. 3D Printing: A Comparative Study
Injection molding and 3D printing are two favored manufacturing technologies used in the creation of plastic items. What Is Injection Molding? Injection molding is a manufacturing process for producing plastic parts in large quantities. It involves injecting molten plastic into a specially designed mold, allowing it to cool and solidify, and then removing the finished part. The process offers high production speed, excellent part quality, and material versatility. However, it requires upfront investme......
Jan 11,2024
White Nylon VS. Black Nylon In 3D Printing: A Comparative Analysis
Material Properties of Both White Nylon & Black Nylon Nylon is widely recognized for its exceptional strength, durability, and flexibility, regardless of the color of the nylon filament. The material properties that make nylon desirable for various applications, such as high impact resistance and good layer adhesion in 3D printing, remain largely consistent between white and black nylon. Both variants should offer comparable mechanical characteristics, ensuring reliable and robust printed objects. The......
Jan 02,2024
How to Decimate the Size of an STL File for 3D Printing
Why is it necessary to reduce the size of an STL file? While large 3D files may not pose a theoretical problem, the practicality of sharing or uploading them may. Overly heavy 3D files may create obstacles such as upload limitations - jlc3dp has a maximum file size of 100 MB.Many overly large files contain intricate details that surpass the capabilities of both human perception and 3D printers. This tutorial aims to address this challenge by demonstrating methods to decrease file size while preserving......
Dec 28,2023
What Is an Appropriate Wall Thickness for 3D Printing Parts
What is Wall Thickness in 3D Printings Wall thickness in 3D printing refers to the distance or thickness of a printed object's vertical walls or surfaces. Importance of Wall Thickness Wall thickness affects the structural integrity, printability, and overall quality of the printed product, making it an important factor to take into account in 3D printing. For example, the wall thickness directly affects the strength and durability of 3D-printed objects. Specifically, a thicker wall provides more struc......
Dec 28,2023