CNC Machining Design Guideline
CNC Machining Design Guideline
CNC machining involves the precise removal of material from a solid block using high-speed rotating cutting tools to achieve desired shapes. The cutting tool plays a crucial role in this process as it directly interacts with the workpiece, eliminating excess material to obtain the final part.
Standard CNC cutting tools, such as end mills and drills, typically feature a cylindrical shank, various tip shapes, and limited cutting length. These characteristics make it challenging to create deep, narrow holes and complex overhangs. To help you save costs by avoiding expensive CNC operations, we have compiled some common design techniques in this article.
Avoiding small internal corners
Due to the cylindrical shape of CNC milling tools, it is difficult to achieve perfectly sharp internal corners. It is necessary to implement thinner tools for smaller corners, resulting in longer machining times and increased fragility, ultimately raising costs.
Therefore, it is advisable to maximize the radius of internal corners. In the absence of specific instructions, sharp internal corners will be machined according to the values shown in the below table based on the corner depth.
Assuming the diameter of the cutting tool is D and the maximum depth of the internal cavity is H, with the minimum internal radius denoted as R, the formula is given as R=(H/10)+0.5 and D=H/5 (unit is in mm). For example, if the internal cavity depth is 30 (mm), the minimum internal radius that can be machined is R 3.5 (mm) with (30/10)+0.5 (mm), and the corresponding cutting tool diameter is 6 (mm) with 30/5 (mm). Currently, we can achieve a minimum internal radius of R 0.5 (mm) with a depth of ≤3 (mm). Smaller internal radii require smaller cutting tools, which can result in higher machining costs.
Max. corner length and min. internal R for different tool diameters
Number | Tool Diameter | Length(mm) | Maximum Length(mm) | Minimum R(mm) |
1 | ⌀ 2.0 | 8 | 10 | 1.5 |
2 | ⌀ 3.0 | 12 | 15 | 2 |
3 | ⌀ 4.0 | 15 | 20 | 2.5 |
4 | ⌀ 6.0 | 25 | 30 | 3.5 |
5 | ⌀ 8.0 | 35 | 40 | 4.5 |
6 | ⌀ 10.0 | 45 | 50 | 5.5 |
7 | ⌀ 12.0 | 55 | 60 | 6.5 |
8 | ⌀ 16.0 | 75 | 80 | 8.5 |
9 | ⌀ 20.0 | 95 | 100 | 10.5 |
10 | ⌀ 25.0 | 120 | 125 | 13 |
11 | ⌀ 32.0 | 155 | 160 | 17 |
12 | ⌀ 50.0 | 240 | 250 | 27 |
13 | ⌀ 63.0 | 305 | 315 | 35 |
Note: Higher lengths are possible with tool holder extensions (not recommended).
If you need to retain sharp corners on the workpiece, please provide a 2D drawing with specific annotations. We offer two options for achieving this:
1. Spark erosion for corner cleaning: This process involves using a CNC machine to create copper electrodes, which are then used in a spark erosion machine to remove material and achieve sharp corners. Please note that this method incurs higher costs.
2. Modifying the workpiece structure with R-angles: By incorporating rounded corners (R-angles) directly into the design, we can machine the workpiece using CNC without the need for additional processes. This approach generally results in lower costs.
In the case where both sides of the workpiece have through holes, we can use an online cutting machine to perform corner cutting. However, please be aware that this method may involve higher costs.
Dimensioning threaded holes
1. To ensure your design intention is clearly understood, we recommend designing threads according to standard major and minor diameters, and fully describing the thread parameters in your order. If manufacturing matching threads (e.g. screw and nut), combine them into a single order so they can be checked by our engineers.
2. Each engineer draws the base drill diameter of the 3D thread differently. For example, the standard diameter of the base hole for M3×0.5 is ⌀ 2.5 (see figure below). In the programming, we drill directly according to the ⌀ 2.5 base hole diameter, then use an automatic tapping machine to tap the thread. If the base hole is drawn as ⌀ 3, it will be too large for thread tapping (some can be remedied with thread inserts).
3. For non-standard threads, it is necessary for the customer to provide physical samples for confirmation.
4. Strong thread connections occur in the first few threads and often do not require very long thread lengths. Long thread holes may require special tools, result in longer processing time, and incur additional costs. The thread length is recommended not to exceed three times of the hole diameter. When the threaded hole is a blind hole, it is recommended to leave an unthreaded length of at least half the hole diameter at the end of the hole.
Depth of cavities
Deep cavities can be very costly to machines, because a large amount of material needs to be removed, which takes a very long time. The cutting length of CNC tools is limited, and the best machining effect is achieved when the cutting depth reaches 2-3 times its diameter. For example, a ⌀ 12-milling cutter can safely produce a cavity up to 25mm deep.
Cutting deeper cavities (5 times or more the diameter of the tool) can cause problems such as tool deflection, difficulty in chip removal, and tool breakage, and therefore require special tools or multi-axis CNC systems. In addition, when cutting cavities, the tool must be tilted to the correct cutting depth, and a smooth entry requires enough space.
The cost can be minimized by limiting the depth of all cavities to five times their length (i.e. the maximum size on the XY plane).
Thin walls
Thin walls in a part require multiple passes at low cutting depths, which can easily lead to vibration, deformation, and breakage. Therefore, thin walls are difficult to machine accurately and take longer to produce.The recommended wall thickness of metal parts should be 0.8 mm (absolute minimum 0.5 mm), and 1.5 mm (absolute minimum 1 mm) for plastic parts.
Tolerances
Smaller tolerances cost more because they take longer to produce and inspect.If no tolerance is provided, parts will be made with standard tolerance (±0.1mm or higher). For other tolerance requirements, a 2D drawing annotated with tolerances must be provided.
2D Drawings
Some aspects of a design might be best conveyed through a 2D drawing. Having requirements clearly specified such as tolerances, surface roughness, assembly between different parts, critical areas, and quality requirements can help our engineers choose the most appropriate manufacturing process and potentially lower the cost of the part.
Threaded holes should be annotated with the thread parameters and depth.
Our review engineers will cross-check any 2D drawings against the 3D model and consult you if there are any discrepancies.
If you are ready to make your CAD files to be machined,get free online quote now!
Last updated on Nov 27,2023