How to choose the right material for your CNC project
How to choose the right material for your CNC project
What is CNC Machining?
Computer numerical control, commonly called CNC is the automated control of machining tools (such as drills, lathes, mills, grinders, routers, and 3D printers) by means of a computer. A CNC machine processes a piece of material (metal, plastic, wood, ceramic, or composite) to meet specifications by following coded programmed instructions and without a manual operator directly controlling the machining operation.
What materials are available in JLCPCB?
CNC machining has become an essential manufacturing process in many industries, providing high accuracy and efficiency in creating parts and products. One of the critical factors that influence the success of a CNC project is choosing the right material for the job.
6061 Aluminum Alloy
6061 aluminum alloy is a popular choice for CNC machining due to its excellent strength-to-weight ratio, high corrosion resistance, and easy machinability. It is commonly used in aerospace, automotive, and electronics applications, among others.
7075 Aluminum Alloy
7075 aluminum alloy is a high-strength material that is commonly used in aerospace, military, and sports equipment applications. It has excellent fatigue resistance and good machinability, but it is more difficult to weld than other aluminum alloys.
T2 Purple Copper
T2 purple copper is a soft, malleable material that is commonly used in electrical and electronic applications due to its excellent conductivity and thermal properties. It is also easy to machine and weld.
H59 Brass
H59 brass is a strong, corrosion-resistant material that is commonly used in plumbing, electrical, and automotive applications. It is easy to machine and has excellent ductility and thermal conductivity.
Epoxy Plate - FR4
Epoxy plate - FR4 is a popular material for PCB (Printed Circuit Board) manufacturing due to its high electrical insulation and excellent mechanical properties. It is also flame-resistant and has good dimensional stability.
Bakelite
Bakelite is a thermosetting plastic that is commonly used in electrical and electronic applications due to its excellent electrical insulation properties. It is also heat-resistant and easy to machine.
Steel-POM
Steel-POM is a strong, lightweight material that is commonly used in automotive and mechanical applications. It has excellent wear resistance, low friction, and good dimensional stability.
ABS Engineering Plastic
ABS engineering plastic is a commonly used thermoplastic material that is known for its strength, durability, and flexibility. It is commonly used in automotive, consumer goods, and electronic applications.
Polypropylene - PP
Polypropylene - PP is a lightweight, flexible thermoplastic material that is commonly used in packaging, automotive, and consumer goods applications. It is known for its excellent chemical resistance and easy machinability.
Nylon - PA6
Nylon-PA6 is a strong, lightweight thermoplastic material that is commonly used in automotive, industrial, and consumer goods applications. It has excellent wear resistance, low friction, and good dimensional stability.
PMMA (Acrylic)
PMMA (Acrylic) is a transparent thermoplastic material that is commonly used in optical and lighting applications. It is known for its excellent clarity, scratch resistance, and easy machinability.
Polycarbonate-PC
Polycarbonate-PC is a strong, tough, and transparent material that is commonly used for plastic lenses in eyewear, medical devices, automotive components, protective gear, greenhouses, Digital Disks (CDs, DVDs, and Blu-ray), and exterior lighting fixtures.
Tips to choose the right materials for your products
With a wide range of materials available, from metals to plastics and composites, selecting the appropriate material for your CNC project can be a daunting task. Here are some tips to help you make the right choice:
1. Determine the Requirements of Your Project
The first step in selecting the right material for your CNC project is to understand the specific requirements of your project. What are the dimensional and tolerance requirements of the parts you need to produce? What are the mechanical and chemical properties that your parts need to withstand? Knowing the answers to these questions will help you narrow down the selection of materials that can meet your project's needs.
2. Consider the Properties of the Materials
Each material has its unique properties, including strength, ductility, toughness, and wear resistance. Here are some general guidelines that can help you select the appropriate material for your CNC products from the list of materials we can provide.
- Aluminum Alloys: If your product requires good strength, high corrosion resistance, and good weldability, then aluminum alloys could be an excellent choice. 5052 aluminum is a good choice for marine applications, while 6061 aluminum alloy is commonly used for machine parts, structural components, and aerospace. 7075 aluminum alloy is a higher-strength alloy, commonly used for aerospace and high-performance applications.
- Copper and Brass: If your product requires excellent electrical conductivity and thermal conductivity, copper and brass could be good options. T2 Purple Copper and H59 Brass are good choices for electrical and plumbing applications, while H62 Brass is commonly used for decorative purposes.
- Composites: Epoxy Plate - FR4 and Bakelite are composite materials with excellent electrical insulation and mechanical strength, making them ideal for electronic and electrical applications.
- Plastics: ABS Engineering Plastic, Polypropylene-PP, Nylon - PA6, Acrylic, and Polycarbonate-PC are all thermoplastics with varying mechanical properties. If your product requires high strength and toughness, then Nylon - PA6 could be a good choice. If you need high-temperature resistance, then Polypropylene-PP may be a good choice. ABS Engineering Plastic is commonly used for automotive and electronic housings, while Acrylic and Polycarbonate-PC are ideal for products that require optical clarity.
- Steel-POM: Steel-POM is a thermoplastic material with good mechanical properties and high wear resistance, making it ideal for bearings, gears, and other mechanical components.
3. Evaluate the Machinability of the Materials
Another crucial factor to consider when selecting the right material for your CNC project is the machinability of the material. Machinability refers to how easy it is to cut and shape the material during the CNC machining process. Some materials, such as Aluminum Alloy, have excellent machinability and can be cut quickly and easily, while others, such as Polycarbonate-PC, require special machining techniques and tools to avoid melting or cracking. It's essential to choose a material that matches your CNC machining capabilities and equipment to ensure optimal results.
4. Consider the Cost
The cost of the material is another critical factor to consider when selecting the right material for your CNC project. Some materials are more expensive than others, depending on their availability, properties, and machining requirements. For example, high-strength materials such as 7075 aluminum alloy and steel may cost more than other materials such as ABS engineering plastic and Nylon-PA6. It's essential to balance the material cost with the desired properties and machinability to choose the most cost-effective option for your project.
In summary, the selection of the material for your CNC products depends on several factors, and it is important to consider the application, required mechanical properties, environmental conditions, and cost before choosing the appropriate material.
If you are ready to make your CAD files machined,Get free online quote.
Last updated on Dec 01,2023