This website requires JavaScript.

What is Stereolithography(SLA)3D Printing

Help Center  /  Stereolithography-SLA  /  What is Stereolithography(SLA)3D Printing

What is Stereolithography(SLA)3D Printing

Stereolithography (SLA)3D printing is a cutting-edge additive manufacturing technology that brings digital designs to life by creating three-dimensional objects layer by layer. This innovative technique, also known as resin 3D printing, utilizes the principles of photopolymerization to craft intricate and precise objects. From functional prototypes to artistic creations, SLA 3D printing has found its application across various industries, revolutionizing the way we manufacture objects.


How does Stereolithography-SLA 3D printing work ?



1. Resin Selection: The process begins with selecting a suitable liquid resin, each designed to impart specific properties to the final object, such as strength, flexibility, or transparency.


2. Layer-by-Layer Building: A vat contains the liquid resin, and a build platform is immersed in it. A high-precision UV laser or light source scans the resin's surface, pinpointing specific areas where the resin is to be solidified according to the design.


3. Selective Photopolymerization: As the UV laser or light source moves across the resin's surface, it triggers a chemical reaction in the resin, causing it to solidify and take the desired shape.


4. Z-Axis Movement: After each layer is completed, the build platform moves incrementally, allowing the next layer of resin to be exposed to the laser. This process is repeated until the entire object is constructed.


5. Post-Processing: Once printing is done, the object is removed from the vat and typically rinsed in a solvent to remove any excess, uncured resin. In some cases, additional post-curing might be performed, subjecting the object to further UV light to ensure complete curing and hardening.


6. Support Structures: Complex designs or overhanging features often require support structures to prevent deformities during printing. These supports are removed after the printing process is complete.



What materials are used for Stereolithography-SLA printing?


SLA 3D printing employs a variety of photopolymer resins that solidify when exposed to specific wavelengths of light, usually ultraviolet (UV) light. These resins come in different formulations to meet various requirements, ranging from mechanical properties to visual aesthetics. Here are some common types of materials used for SLA 3D printing:


1. Standard Resins: These resins are versatile and suitable for general-purpose 3D printing. They offer a good balance of detail resolution and mechanical strength, making them ideal for a wide range of applications.


2. Engineering Resins: These resins are engineered to have enhanced mechanical properties such as high tensile strength, impact resistance, and heat resistance. They are commonly used for producing functional prototypes, engineering parts, and components that need to withstand stress.


3. Flexible Resins: Flexible resins create objects with rubber-like properties, allowing them to bend, stretch, and compress. These materials are used for creating products like gaskets, hinges, and parts that require a degree of flexibility.


4. Transparent Resins: Transparent or clear resins produce objects with high optical clarity, making them suitable for applications that require see-through components, like lenses, light guides, and transparent prototypes.


5. High-Temperature Resins: These resins can withstand elevated temperatures without deforming or losing their mechanical properties. They are used in applications where parts will be exposed to heat, such as under-the-hood automotive components or functional prototypes for high-temperature environments.


6. Biocompatible Resins: Biocompatible resins are designed for medical and dental applications. They are safe to use in contact with the human body and are commonly used to create dental models, surgical guides, orthopedic devices, and hearing aids.


7. Castable Resins: Castable resins are used to create objects that can be used in investment casting processes. They burn out cleanly during casting, leaving behind a mold cavity that can be filled with molten metal.


8. Jewelry Resins: These resins are tailored for creating intricate and detailed jewelry pieces. They often provide high detail resolution and smooth surface finishes, making them popular among jewelry designers.


9. Color Resins: Some SLA printers can use color resins to produce objects with full-color capabilities. These resins are used to create vibrant and multicolored prints without the need for additional post-processing steps.


10. Elastic Resins: Elastic resins produce objects with stretchable and rubber-like properties, similar to silicone rubber. They are used for creating wearable devices, flexible connectors, and other stretchable components.



What are the advantages of Stereolithography-SLA 3D printing?


SLA 3D printing boasts several compelling advantages:

1. Precision: SLA technology excels in producing intricate and highly detailed objects with exceptional precision, making it ideal for applications that demand accuracy.


2. Smooth Surface Finish: Objects printed using SLA have smooth surfaces and fine details, reducing or even eliminating the need for post-processing.


3. Diverse Material Properties: The availability of various resin types offers a wide spectrum of material properties, enabling customization for specific purposes.


4. Complex Geometries: SLA can effortlessly handle complex geometries, overhangs, and delicate structures that might be challenging for other 3D printing methods.


5. Applications: SLA finds its place in industries such as jewelry, dentistry, engineering, and product design, where intricate details and high-quality finishes are paramount.



What are the disadvantages of Stereolithography-SLA 3D printing?


Despite its strengths, SLA 3D printing comes with some limitations:

1. Speed: The layer-by-layer process can be time-consuming, especially for larger objects, making it relatively slower compared to other 3D printing methods.


2. Material Costs: Resins used in SLA printing can be more expensive compared to filaments used in other methods like Fused Deposition Modeling (FDM).


3. Post-Processing: While SLA objects often require less post-processing, removing support structures and ensuring proper curing can still be time-intensive.


4. Limited Build Size: The size of objects that can be printed is constrained by the build platform's dimensions, which might limit the feasibility of large-scale projects.


5. Less Mechanical Strength: While SLA prints are precise and detailed, they might have slightly lower mechanical strength compared to prints made using some other methods.



What materials are included in JLCPCB's SLA 3D printing?

SLA-LEDO 6060 - Photosensitive Resin

SLA-9000R - Photosensitive Resin

SLA-8001 - Photosensitive Resin

SLA-8228 - Photosensitive Resin

SLA-Black Resin- Photosensitive Resin

SLA-8111X - Photosensitive Resin

Are you ready to make your 3D files 3D printed? Get instant quote now!

                                                             

Last updated on Dec 20,2023